Green and sustainable profitability with heat recovery
Axel Månsson is one of Denmark’s leading producers of organic vegetables and eggs. The 40+ year old company places premium on quality and fresh…
エラーが発生しました。後でもう一度試して下さい。
Axel Månsson is one of Denmark’s leading producers of organic vegetables and eggs. The 40+ year old company places premium on quality and fresh…
The Spanish company Camposotillos in Toledo runs dairy cattle farming and forages for its own consumption. It was founded in 2004 an initiative of…
Carl von Linné is the father of modern taxonomy as he laid the foundations for the modern scheme of binominal nomenclature. During his studies in…
Crown Perth (formerly known as Burswood Entertainment Complex) is located on the Swan River near the city of Perth, Western Australia, and is owned…
With Munters’ mass transfer expertise, a customer in the steel industry was able to improve their column performance with optimized chilled water…
Since data centers require a sustainable design, the cooling system is often a primary concern for designers and operators. This is because the …
Deep within the picturesque Colli Eganei (Euganean Hills) lies Europe's first botanical garden. Nestled in this idyllic region, in the town of…
In August 2015 the new public bath Hyllie opened in Malmö. A brand new facility with Eco-thinking and the ambition to be Sweden's most energy…
Kolafabriken in Bräkne-Hoby, Sweden was founded back in 1993, when the company took over some discarded production machinery from a caramel factory.…
The German supermarket chain Lidl dates back to the 1930s. The first Lidl store opened in 1970 and today there are more than 10,000 Lidl supermarkets…
The strength and versatility of a major shipbuilder in the Netherlands lies in its ships, which are custom built. For over 150 years, they have…
Rising energy costs and shortages around the world have driven the power and process industries to seek innovative solutions. Worldwide energy demand…
When it comes to delivering efficiency, Munters set the bar with its patented Munters Drive motor technology released in 2008. Today, Munters…
A creamery located in the Midwest required a replacement heater for one of their spray drying systems that processes powdered milk, and the new…
Nestec, Inc. provided two 46,000 standard cubic feet per minute (SCFM) Regenerative Thermal Oxidizer (RTO) systems to a potato processing facility in…
Pharmadule, the world leader in modular manufacturing facilities for the pharmaceutical industry, has in recent years been working with Munters to…
A manufacturer of nitrobenzene and other petrochemicals enhanced their column capacity and increased nitrobenzene recovery from the effluent with…
ワシントン州クインシーにあるSabey社のデータセンターは、付近を流れるコロンビア川の水力による低コストの供給電力を活用した、同種の6つの大規模データセンターの1つです 。…
Munters has been working closely with metal industries throughout the world for many years and developed several solutions for mist elimination in…
Volsgård I/S is owned by Torben Thorsen and Vagn Rasmussen. Volsgård is a family farm belonging to Vagn’s family. Vagn is a 4th generation farmer.…
A Wisconsin printer that uses flexographic printing equipment was experiencing air balance problems at their printing plant. Drafts and high energy…
Claxton Poultry had issues with condensation in its production facility, and needed to look for a reliable, efficient solution. Munters proposed a…
世界最大のデータセンター企業のひとつであり、コロケーションプロバイダー(顧客のサーバを預かり、通信回線や保守サービスを提供する業態)であるエクイニクスは、オーストラリアのメルボルンに初のME1データセンター(以下、ME1)を開設、そしてロンドンのスラウに6番目となるデータセンターLD6(以下、LD…
TC Energy pumps natural gas through underground pipelines from production facilities in western Canada to consumers in eastern Canada and the Midwest…
Humidity causes fog, condensation, mildrew, odours and rust. Munters desiccant dehumidification systems remove moisture from the air and eliminate…
IKEA worldwide aims to become greener. A more sustainable environment is an important global responsibility.
米国オレゴン州にある電子系自動設計ソフトウェアのリーディング・カンパニーMentor Graphics…
Cold weather provides a unique set of problems to the efficient operation of equipment and processes, whether land-based, offshore, or marine. To…
Munters solved an emergency high pressure drop and bottom temperatures issue for a customer in the petrochemical industry. Munters technicians…
Laing O’Rourke, Munters and Faber Maunsell have completed a main cable dehumidification system on the center spans of the Severn Suspension Bridge…
デンマークは2006年に2570万頭の豚を生産し、世界一の豚肉の生産量と輸出を誇ります。(生産された豚肉の85%が輸出され、それはデンマーク全体の輸出総額の5.3%を占めます。)デンマークでは家族経営の農場は一般的で、養豚場も例外ではなく、7800箇所もあります。エスパン・ドレープ氏が所有するソル…
A major international pharmaceutical company manufactures prescription medications and specializes in cancer care products. Their production process…
Akıncı Tavukçuluk Ltd. Şti. was founded in 1998. The farmland occupies 56.000 m2 with 9 buildings having a total surface of 11.000 m2 closed area and…
At British Sugar, Cantley, UK, 1,350 tonnes of sugar are produced every day. After the sugar crystals are washed, dried and cooled, they are conveyed…
イタリア、シチリア島の南に位置するラグーザ県は、バロック建築の美しい街並みが広く知られ、ユネスコの世界遺産にも登録されています。そのなかでも街全体が世界遺産に指定されているシクリは人口2万6千人で、イルミニオ川の河口からピショット地区まで約20キロに渡る地中海の沿岸に広がり、高品質のトマトの生産地…
Crawford Equipment & Engineering Company of Orlando, Florida offers a complete line of services related to industrial process heating equipment,…
The ice rink Ijsbaan Leuven located in Belgium hosts a wide range of activities, from ice hockey to figure skating and disco skating. The arena can…
General practice in the food industry and particularly in the distribution of frozen products is to increase stock rotation without increasing…
In 2013 Germany’s first fully automated cold store was built by KLM Logistic in the city of Rheine in north western Germany. Munters was able to…
The PolyPeptide Group is involved in all major peptide technologies and handle peptide production from small-scale (multi-10 mg) non-GMP batches to…
Energy saving, low dewpoint conditions for advanced battery system dry rooms at QinetiQ.
The idea began with a request from Padre Economo, who is an existing Munters customer, who uses two MLT800s for climate control in his library. He…
A leading ammonia manufacturer increased their plant capacity by 20% using Munters’ mass transfer equipment.
India’s largest producer of formic acic, acetic acid and methanol asked Munters to solve a problem they were having with dislodging trays during…
The Simon family operates a small dairy farm in the vicinity of Garibaldi, Rio Grande do Sul in Brazil and maintain a herd of 77 cows. Summer…
In 2015 Archive Centre Blekinge inaugurated their new facilities, which contain more than ten kilometers of shelfs held in a two story building in…
Nestled in Two Wells, South Australia, the d'VineRipe tomato glasshouse complex exemplifies innovation in sustainable agriculture. Faced with the…
The IceDry® frost prevention method has been developed by Munters for use in freezing and storage facilities, resulting in faster freezing,…
Gemlik Gübre is Turkey´s largest fertilizer manufacturer. Based in Bursa, they produce various types of fertilizers, and export 65% of their…
The Mary Rose is the only 16th century warship on display in the world, built between 1509 and 1511, she was a firm favourite of King Henry VIII. She…
The demand for sugar continues to rise faster than supply, and the shortage has created a demand that requires sugar producers to be more efficient.…
Production of hormone medication involves packing into foil blister packs. The process also includes cooling and therefore entails very cold machine…
Third-generation farmers, and owners of Iowa Select Farms, Jeff and Deb Hansen, started with humble roots in 1976, farrowing just three sows. Through…
Munters´ mass transfer solutions helped one of the top three largest producers of glycerin and fatty acid in India reduce utility consumption by 20%…
Treating contaminated soil efficiently poses a tremendous challenge for environmental specialists, but TerraTherm, an environmental services company…
The Van Ess Dariy farm located in Sanborn, Iowa, is run by five brothers and overseen by their parents, Harvey and Lisa Van Ess. The family saw an…
Colorado’s Farm is located in Araras City in São Paulo State. The company was founded in 1982 and is one of the biggest milk producers in the…
Gasmac Incorporated of Ontario, Canada manufactures painting systems used in industrial plants, and the company features Munters air-to-air heat…
The University of Münster, Germany MEET battery competence center employs an international team of over 150 scientists. MEET brings together basic…
Located in Gentofte, Denmark, the Phistergården day care is an independent institution with forty children from three to six years old. It´s housed…
A leading manufacturer of petrochemicals in India reduced their LAB slippage to less than 5% and improved its Acid Color Index, which measures the…
WMG’s Energy Innovation Centre features a battery characterization lab and an electric/hybrid drive testing facility. The Centre features a…
In smaller chilled stores used by laboratories, catering facilities, and restaurants, the naturally high-relative humidity causes problems quite…
Halim Co Ltd. (founded in 1978) is the biggest company in the Korean broiler industry and employs a complete integration system comprising farming,…
During the warmest 4 months of 2012, a comparative test was done between two identical growing/finishing barns in the South-East of Brazil. The aim…
A fertilizer plant customer was facing serious problems with liquid carryover. Munters suggested two different solutions and solved the problem…
The Kalgoorlie Courts Project includes three magistrates’ courts, two jury courts and a range of mediation, registry and other support facilities.…
The Albany Entertainment Centre is a state of the art performing arts and convention centre with a stunning waterfront location like no other in…
Swedish AB Cernelle is the founder of superior pollen extracts for medical treatment. Started in 1953, the company had a vision that purified…
Production of broiler meat in Spain has increased 2% in 2010 from previous year, and the country consolidates its position among one of the top 5…
One of the largest fish groups A. Espersen A / S in Ronne, saw how IceDry® has clearly improved conditions in their freezer area.
Cobb is a poultry research company engaged in the development, production, and sale of broiler breeding stock. This is one of the most important…
Japan is an island chain in Eastern Asia, between the North Pacific Ocean and the Sea of Japan, and east of the Korean Peninsula. Its climate varies…
Milking cows are very sensitive to heat stress and typically suffer from reduced milk production and conception rates during hot periods.
Nestled within Turkey's Toros Agripark lies a haven for disease-free, high-yield banana plantations. The secret behind this success? A…
高品質のバラ生産ビジネスを手掛けるスペインの Rosas Elig-Florは、Elig-Flor CastallaとRosas Campello Obiol による合弁会社で、2社の連盟会社がアリカンテのエルチェ市(Elche)とカスタジャ市(Castalla)に生産拠点を構えています。
In Northern Africa, bordering the Mediterranean Sea, between Algeria and Libya, lies the Republic of Tunisia. The country has a yearly production of…
ジェリー・オブライアンは70年代半ばに養豚場経営を始めました。80年代半ばには、エアロテックの営業であるラルフ・レターズと事業を開始しました。ジェリーとラルフの協業により、今日では125棟の畜舎と1万頭以上の豚を擁する大規模な養豚事業に成長しました。創業後30年、ジェリーの息子のJW・…
ユーザーIDが正しくありません。
エラーが発生しました。後ほどもう一度お試しください。
パスワードをお忘れですか?
ユーザーIDが正しくありません。
エラーが発生しました。後ほどもう一度お試しください。
Check your email within a couple of minutes to reset your password, if you can’t see any incoming messages try to check into your spam folder!