Une erreur occursée lors de l'envoi du message, s'il vous plaît essayer à nouveau plus tard
Une erreur occursée lors de l'envoi du message, s'il vous plaît essayer à nouveau plus tard
Munters utilizes sophisticated software combined with extensive experience in livestock ventilation to generate a design proposal to suit any farm for farrowing, gestation or finisher pigs. The result will not only specify the right equipment to deliver the required airflow, but will also deliver increased profit margins for growers and farmers, here is how.
An adequately designed ventilation and climate control system will provide the farmer with numerous benefits. To start with it is important to mention that the single highest cost for the pig farmer is the feed to the animals. This consists of 60-70% of the producer costs. Therefore it is of essence that the pigs, especially finishers, can convert the consumed feed into body mass (feed conversion ratio) in the most optimal way. We don’t want the scenario where feed and energy intake is consumed to keep the animal cool or warm it up. But that is not the only reason to have a proper air exchange rate, circulation of air or heating in cold periods. The pigs’ health and welfare also strongly depend on this, as does the health of the staff working in the barn. By keeping the animals in a sound and closed, climate controlled environment and maintaining good bio security measures, there is less need to give the pigs medication, which saves money for the farmer or grower. All in all, a perfect climate for swine or hog farming provides environmental excellence, increases profits for the contract grower and gives a healthier meat product for consumers.
The environment in the barn comprises box fans, chimney fans or cone fans assuring adequate air quality, air speed, ventilation capacity and air exchange rate to maintain air quality and avoid heat stress. In colder climate zones, minimum ventilation rate is crucial to avoid suffocation of the pigs and ensure a good working environment for farm staff. At times additional heating might be necessary. Correct temperature must be kept in relation to the swine production stages, avoiding temperature swings and maintaining a uniform climate inside the barn. Ammonia emission control can be instrumental in densely populated areas when the farmer wants to be able to expand the farm. Munters are pioneers in ammonia air cleaning without filter material that can get clogged up. The MAC air cleaner is based on droplet separation technology, which can easily be cleaned regularly with a high pressure cleaner by the farmer himself.
Humidity, methane, ammonia and other gases all together contribute to one of the harshest environments there is today in modern livestock farming. Munters have figured out a way of dealing with it and help farmers create their perfect climate. Munters Protect is a coated steel with extremely good resistance performance. In fact its protection factor is 10 times better than standard galvanized steel fans. Since 2014, all metal fans produced in our Italian factory are manufactured in Munters Protect.
After all, the optimal climate will materialize itself as more money in the pocket for the farmer or grower.
Munters is recognized and well reputed for its product brands CELdek®, Euroemmme® and Aerotech®.
Identifiant invalide
Oups! Une erreur est survenue. Essayez plus tard.
Mot de passé oublié?
Identifiant invalide
Oups! Une erreur est survenue. Essayez plus tard.
Check your email within a couple of minutes to reset your password, if you can’t see any incoming messages try to check into your spam folder!