Une erreur occursée lors de l'envoi du message, s'il vous plaît essayer à nouveau plus tard
Une erreur occursée lors de l'envoi du message, s'il vous plaît essayer à nouveau plus tard
The »Heat-X« type DG is a directly fuelled fan heater with a stable flame for the clean, complete combustion in connection with low energy consumption.
Optimal stable temperatures have a large influence on the health and efficiency of the animals. As a result, in many climatic regions the use of a heater is essential. In addition to the correct temperatures, the uniform air dis-tribution is a further important factor in order to achieve the best possible conditions both in agriculture as well as in horticulture.
The »Heat-X« type DG was specifically devel-oped in order to control these factors.
The air volume of 6,000 – 7,000 m3/h attuned to the heating capacity and the special, conical outlet of the fan heater pro-vide an optimal air distribution, which safe-guards the even heat distribution and
a uniform climate.
The »Heat-X« type DG is suitable for different fuels and can be delivered in the following versions: Natural gas (H-gas and L-gas), butane, propane or liquefied petroleum gas. The fan heater is set to the desired fuel at the factory. Alternatively, a conversion kit is available, with which the gas type can be set on-site.
Disponible en Sweden, Spain, Denmark, France, Italy, Russia, Germany, Poland, Belgium, Austria, Belarus, Ukraine, Europe, Middle East, Africa
Identifiant invalide
Oups! Une erreur est survenue. Essayez plus tard.
Mot de passé oublié?
Identifiant invalide
Oups! Une erreur est survenue. Essayez plus tard.
Check your email within a couple of minutes to reset your password, if you can’t see any incoming messages try to check into your spam folder!