Ha ocurrido un error cuando se ha enviado el mensaje, por favor, inténtelo más tarde
Ha ocurrido un error cuando se ha enviado el mensaje, por favor, inténtelo más tarde
Applying fertilizer while watering plants through an irrigation system is a precise and efficient way to deliver nutrients. Fertigation can help improve crop yield and quality. Explore how fertigation can maximize the potential of plants within controlled environments while conquering nutrient challenges.
Applying fertilizer only when needed enables growers to realize savings and reduce their environmental impact. Using the controller also lets growers implement advanced fertigation strategies, such as:
Fertigation and climate control are closely interconnected. For example, greenhouse temperature and humidity can affect the nutrient uptake of plants. Similarly, the nutrient levels in irrigation water can affect a plant’s ability to withstand stress.
By carefully managing fertigation and climate control, growers can optimize the growing environment for their plants. The result? Increased crop yield, improved crop quality and reduced crop losses. Moreover, they can extend the growing season, reduce energy costs and introduce more sustainable practices to their greenhouses.
Fertigation techniques possess the remarkable ability to cater to the distinct nutrient needs of various crops. This adaptability is at the core of successful greenhouse cultivation.
For instance, a leafy greens crop may require a higher nitrogen-to-phosphorus ratio, while flowering plants like roses thrive with elevated potassium levels. A vegetable crop like tomatoes benefits from specific nutrient combinations during its flowering and fruiting stages, leading to plump and flavorful yields. By tailoring the nutrient mixture to the requirements of each crop, plants receive what they need for optimal growth and development.
As plants progress through different growth stages, their nutritional demands shift significantly. This prompts the need for nuanced adjustments in nutrient ratios and applications.
During the early stages, plants require a nutrient boost for strong root and shoot development. As they transition to vegetative growth, higher nitrogen ratios fuel lush foliage.
Finally, as they enter the flowering and fruiting stages, a shift towards higher phosphorus and potassium levels supports bloom production and robust fruiting.
Fertigation's responsiveness allows growers to tailor nutrient delivery precisely, aligning with the requirements of each growth phase.
Enviaremos su consulta al contacto de Munters de su país
Identificación de Usuario Inválida
Ups! Algo salió mal. Por favor intenta nuevamente
¿Olvidaste tu contraseña?
Identificación de Usuario Inválida
Ups! Algo salió mal. Por favor intenta nuevamente
Check your email within a couple of minutes to reset your password, if you can’t see any incoming messages try to check into your spam folder!