Der opstod en fejl under afsendelsen af beskeden, prøv igen senere
Der opstod en fejl under afsendelsen af beskeden, prøv igen senere
In agriculture applications an ideal climatic environment is essential as it can impact production and the health of animals. Proper air quality through ventilation is one of the main requirements in order to achieve optimum performance in growth rate, uniformity and feed efficiency, which can therefore ensure high profit margins.
Poor air quality can provoke high concentrations of dust, ammonia (NH3), CO, CO2, excess humidity RH and failure to keep these contaminants below acceptable limits can trigger diseases, alter litter quality and reduce bird performance, thus affecting the final profit margin.
The MWI has been engineered and designed to bring fresh air into the farms, without exposing the animals to cold air draughts. This is possible due to the feature of the MWI that offers a complex geometrical shape, that takes advantage of the Coanda effect, to properly channel the incoming cold fresh air along the ceiling, which is mixed and heated before it reaches the animals.
The MWI has been developed to focus on the Broiler industry, however there is a potential for other Poultry application e.g. breeder, layer, turkey.
For more details explore the MWI and learn how to assemble the product in 2 min by watching the following videos:
Ikke valid bruger identifikation
Ups! Der er noget gik galt. Prøv igen senere
Glemt password
Ikke valid bruger identifikation
Ups! Der er noget gik galt. Prøv igen senere
Check your email within a couple of minutes to reset your password, if you can’t see any incoming messages try to check into your spam folder!