Please let us help you

You have to accept our privacy policy to send your request.

Ask a question

Commercial & Public Buildings

Commercial & Public Buildings

Commercial and public buildings must protect the health, safety and general well-being of those occupying the space.

Public places require a certain percent of outdoor ventilation air. However, the humidity and temperature must be maintained at a precise and constant level. Unwanted moisture affects the entire building from the actual structure to its occupants and their health.  Insufficient humidity control results in moldy supplies such as books, and structural decay such as damaged carpet and warped flooring.  Poor indoor air quality (IAQ) leads to headaches, fatigue, asthma (and other respiratory-related problems), an inability to concentrate making for a less productive workplace. Sometimes commercial office space dehumidification is needed because they have archive storage or private fine art collections that need to be protected to prevent against deterioration.

Cooling and maintaining a comfortable environment in an airport is challenging. The large quantity of people walking in and out, and the opening and closing of doors, creates an unpredictable load for an HVAC system to process (and doing so efficiently is even more challenging). Airports must meet Indoor Air Quality (IAQ) regulations that require a certain amount of outside air to be continually brought into the space. They must also maintain certain levels of air pressure to avoid the entrance of Carbon Monoxide (CO). By using Munters energy efficient technology to control temperature and humidity in the airport, IAQ standards are met, more comfortable air is delivered to the space and energy cost savings are realized.

Indoor air quality is a growing concern for everyone. Munters equipment utilizes energy recovery and humidity control technology and can supply the proper amount of fresh, healthy outdoor air at the precise temperature and humidity necessary for any retail or office space.

Solutions

Case studies