Munters DSS Pro offers the next level of dehumidification
Jul 7, 2021
Suitable for indoor or outdoor installation, Munters DSS Pro is designed for a wide range of industries that demand dehumidification efficiencies such as pharmaceutical, food, and battery applications.
Equipped with the Munters custom configured control system, the DSS Pro offers full function integration, delivering the perfect climate whenever and wherever it´s needed. It comes in twenty configurable sizes with three different desiccant rotor types.
The DSS Pro offers key energy-saving features. It consumes up to 30% less energy with its Green PowerPurge™ and when it’s time to transition to renewable energy the DSS Pro is ready for a seamless switch.
Another positive energy saving feature is the new AirPro casing, an innovative enclosure that significantly improves durability, reduces air leakage, and reduces energy consumption.
When it comes to size, the DSS Pro offers a reduced physical footprint, which makes the system more convenient to install and can free up much-needed space that can be used to generate revenue.
Munters offers more than a benchmark dehumidification system with the DSS Pro. As a partner with the knowledge and expertise to ensure indoor climate is always exactly as it needs to be, Munters provides support from design and quotation to ongoing service from our offices all over the world.
“DSS Pro provides reliable and consistent operations, reduced system footprint and a positive effect on the bottom line”, says Sander Hielkema, Product Manager Systems EMEA, Munters. “Our innovative and intuitive selection tool Genesys ensures you get the right Munters solution for your specific needs. It delivers all the technical specifications for installation, start-up and lifecycle of the product, right from the start. Changes are easily made with this smart tool, and we can serve our customers better and more efficiently. Developed for Europe and Asia, the system is the result of a true team effort with the world’s best climate control engineers partnering with our customers to make this a reality,” concludes Sander Hielkema.
For media / press enquiries
Anja Simonsson
Global Marketing Director
Phone: +46 70 255 3694
E-mail: anja.simonsson@munters.com
About Munters Group
Munters is a global leader in energy efficient air treatment and climate solutions. Using innovative technologies, Munters creates the perfect climate for customers in a wide range of industries. Munters has been defining the future of air treatment since 1955. Today, around 3,500 employees carry out manufacturing and sales in more than 30 countries. Munters Group AB reported annual net sales of more than SEK 7 billion in 2020 and is listed on Nasdaq Stockholm. For more information, please visit www.munters.com.
Find out more here.

dss_pro_pr_845x475.jpg?v=638435151210000000