お問い合わせはこちらへ

エラーが発生しました。後でもう一度試して下さい。

ご質問はお問い合わせください

Broiler chicken drinking water

Increased selling price per bird with 47%

Halim Co Ltd. (founded in 1978) is the biggest company in the Korean broiler industry and employs a complete integration system comprising farming, processing and marketing. Today Halim operates around 600 broiler farms (each with a capacity of 40,000 to 50,000 birds per flock) and 60 breeding farms. Combined annual production is 110,000,000 broilers, which are sold into two market categories: fresh meat products and processed meat products.

At the heart of a Munters Climate Control System are two of the most trusted brands in the industry, CELdek ® evaporative cooling pads and Euroemme® fans. The CELdek® evaporative cooling pads are used in systems where high efficiency cooling is required. It can be used in many different cooling applications and is particularly suitable for the
cooling of livestock buildings. Market leading Euroemme® extraction fans are famous for their high energy efficiency; outstanding production quality; tight sealing shutter design and the centrifugal shutter opening system allowing an un-obstructed air passage. Munters climate control systems include a large variety of equipment to provide the best growing environment from the Poles to the Equator. Air heaters for cold regions or cold spells during the year. A full range is offered with a variety of designs and fuel types. Air inlets to facilitate even air distribution during low ventilation rates, suitable for all construction styles. Light filters for all ventilation openings, reducing the light intensity inside
the house sufficiently to be able to utilise artificial daylight programs to full effect. Air blowers/circulators to optimize air homogeneity. Heated air can be distributed evenly to reduce heating bills. Controllers to orchestrate activity of all the equipment to create a harmonious functioning house and the best conditions for growth.

Paying Special attention to climate control and air quality.

Recently Halim invested in yet another broiler farm in the vicinity of scenic Jinan, approximately 200 km south of the capital Seoul. State of the art technology was specified in an effort to improve production efficiency. Special attention was paid to climate control and air quality, consequently a fully automated climate control system was specified.

The investment paid off

Munters rose to the challenge and supplied a complete climate control package comprising: Euroemme fans; CELdek cooling pads; WDP water distribution system for the CELdek pads; IW air inlets; LFd light filters; and FarmPremium climate controller. The investment paid off! Ever since the first growout of broilers, performance data proved the new farm far significantly outperforms the average farm within the Halim group.

情報

  • Improved feed conversion ratio
  • Increased broiler weight
  • Healthier animals
  • Higher revenues for the farm

お困りですか?

会員登録はこちら
クッキーポリシーを許可するにはこちらを選択してください。 クッキーポリシー

ユーザーIDが正しくありません。

エラーが発生しました。後ほどもう一度お試しください。

ユーザーIDが正しくありません。

エラーが発生しました。後ほどもう一度お試しください。