Please let us help you

You have to accept our privacy policy to send your request.

Ask a question

Greenhouse fertigation

Applying fertilizer while watering plants through an irrigation system is a precise and efficient way to deliver nutrients. Fertigation can help improve crop yield and quality. Explore how fertigation can maximize the potential of plants within controlled environments while conquering nutrient challenges.

Strategies for reducing fertilizer waste

Applying fertilizer only when needed enables growers to realize savings and reduce their environmental impact. Using the controller also lets growers implement advanced fertigation strategies, such as:

 

  • Variable rate fertigation uses sensors to monitor the soil nutrient levels and adjust the fertilizer application rate accordingly. Doing so helps ensure plants always receive the optimal amount of nutrients while minimizing fertilizer waste.
  • pH control using the controller to monitor and control irrigation water pH values. This helps ensure nutrients are available in a form that plants can easily absorb. 
  • Nutrient injection precisely controls the nutrients dosed directly into the irrigation water, a precise, efficient way to promote plant growth.

 

Explore other digitally powered solutions

AdobeStock_422437991_mod.jpg

Combining fertigation and climate control

Fertigation and climate control are closely interconnected. For example, greenhouse temperature and humidity can affect the nutrient uptake of plants. Similarly, the nutrient levels in irrigation water can affect a plant’s ability to withstand stress.

 

By carefully managing fertigation and climate control, growers can optimize the growing environment for their plants. The result? Increased crop yield, improved crop quality and reduced crop losses. Moreover, they can extend the growing season, reduce energy costs and introduce more sustainable practices to their greenhouses.

 

Learn more about greenhouse climate control

AdobeStock_437407655_mod.jpg

Crop-specific solutions

Fertigation techniques possess the remarkable ability to cater to the distinct nutrient needs of various crops. This adaptability is at the  core of successful greenhouse cultivation.

For instance, a leafy greens crop may require a higher nitrogen-to-phosphorus ratio, while flowering plants like roses thrive with elevated potassium levels. A vegetable crop like tomatoes benefits from specific nutrient combinations during its flowering and fruiting stages, leading to plump and flavorful yields. By tailoring the nutrient mixture to the requirements of each crop, plants receive what they need for optimal growth and development.

Lapietra greenhouse-14-1.jpg

Growth stage considerations

As plants progress through different growth stages, their nutritional demands shift significantly. This prompts the need for nuanced adjustments in nutrient ratios and applications.

During the early stages, plants require a nutrient boost for strong root and shoot development. As they transition to vegetative growth, higher nitrogen ratios fuel lush foliage.

Finally, as they enter the flowering and fruiting stages, a shift towards higher phosphorus and potassium levels supports bloom production and robust fruiting.

Fertigation's responsiveness allows growers to tailor nutrient delivery precisely, aligning with the requirements of each growth phase.

AdobeStock_204070496.jpg

Solutions

Case studies