AT_Case_salmon1.jpg

Munters IceDry® system keeps the coldstore free of ice and frost!

Munters installed their IceDry® dehumidifiers, which distribute dry, dehumidified air via channels with nozzles down over the door into the air lock. At night, when the door to the production unit is closed, there is an electronic hygrostat to make sure that the dehumidifier is not used unnecessarily.

Installing a Munters IceDry® system meant the dew point lies below the prevailing temperature, which considerably reduces the formation of ice and frosting on the evaporator. This reduces icing up of the refrigeration components, evaporator and condensation tray. Were this not the case, valuable energy and time would be expended on defrosting.

The IceDry® system ensures that the dew point lies below the prevailing temperature within the store. The dry air is fed back into the airlock, combating the formation of ice and frosting. All in all, this saves costly energy and time, and minimises the risk of accidents.

J.P. Salmon A/S has definitely benefited from installing this system. The door now works without problems and can be shut tight as there is no longer any ice damage.

The floors are also dry and safe. Valuable time and money is no longer spent removing ice and frost and equally important are improvements in the safety aspects.

The visibility has improved in the lock area and it is possible to see through the viewing panels.

Why not look on www.munters.com/food for a wealth of case studies.

J.P. Salmon A/S, located in Denmark operates both as a smoke house and production unit. It has 120 employees to process salmon, halibut, trout, and tuna etc., which are sold all over the world.
Between the production unit and cold store, the cold air from the freezer met the warmer and more humid air from the production unit, which resulted in both practical and safety problems.
There were problems with the doors icing up, which meant that they could not be closed properly, while in the actual cold storage room there were large amounts of ice and frost, which had to be cleared from the floor using shovels.
There were also visible signs of major frost damage to the ceiling and evaporators. There were problems with safety in the lock area due to wet, slippery floors and fog.

事实浏览

  • Prevents ice damage to the door, which can cause disruption
  • Prevents fog from forming in the lock areas
  • Allows you to see through panels that were once opaque
  • Prevents floors from becoming wet, slippery and dangerous
  • Prevents frost and ice damage on the ceiling and to products

我们该怎样帮助您?

By selecting you approve our cookie policies

农业环境控制

/sites/default/files/2020-08/20191203103950599.jpg

MUNTERS HELP FEED THE WORLD

//vod.munters.cn/f47e6eec4cd443bbb2b0361e0fd6ff29/01bb032cc029a327faca626ffab6b4c6-sd.mp4

猪舍

蒙特在设计生产猪舍内气候控制设备、系统方面拥有丰富经验。设计适当的通风系统将为猪(肉猪)和饲养员提供适宜的生存环境和工作环境。无论是产仔舍、孕猪舍或育肥舍,更佳的温度、湿度控制及良好的换气系统都是保持禽畜健康和产量的重要因素。

鸡舍

蒙特在设计生产鸡舍内空气处理机组和环控系统方面拥有丰富经验。无论舍外出现何种极端或多变的气候条件,为禽舍专门打造的蒙特通风系统都能轻松而精准地控制舍内的气候环境。

牛舍

蒙特在设计生产牛舍气候控制系统方面具有有丰富的经验。无论舍外出现何种极端或多变的气候条件,为牛舍专门打造的蒙特通风设备都能轻松实现对舍内气候的精准控制。

温室

蒙特研发并制造温室专用的节能型气候控制系统。我们的解决方案可提供更适宜的气候,从而使农户在更佳的状态下开展经营和生产活动。创新型产品系列包括通风产品、蒸发降温产品和加热产品。