Create Environment Awards
Munters Spain among the top 20 sustainable companies in Las Rozas (Madrid) is awarded the “Crea Medioambiente Certification” for its commitment with the Environment and Energy Efficiency.
The Mayor of Las Rozas, José Ignacio Fernández Rubio, delivered The Crea Medioambiente Certifications to 20 companies based in the municipality of Las Rozas who were committed to the implementation of environmentally friendly practices.
The certifications are part of the Life Project "Las Rozas for the climate" and it is funded by the European Union. The Crea Medioambiente Institute, Member of the City Council in this project, certifies the chosen companies that are worthy of this award to fulfil their commitment in the field of Social Responsibility, Environmental and Energy Efficiency.
The Crea Medioambiente Institute has granted this distinction to Munters for the development of the Oasis system that achieves a reduction of energy consumption by up to 75% in data centres.
"The granting of this certification is recognition of Munters’ commitment to the environment and ecological awareness. In addition, being an excellent image and communication tool to differentiate ourselves from our competitors".