IMG_1783.jpg

Munters Protect the barrier against corrosion

7 4, 2014

Munters moves away from galvanized steel for the metal fan line and now launches Munters Protect. The implementation of the new anti-corrosion material forms another step in Munters quest of safeguarding that our products stand the test of time and last in the environment where they are placed, while ensuring that the environmental footprint is reduced.

Step by step with continuous improvements

The agriculture environment is challenging to metal products and corrosion is caused by many factors such as pH, high humidity levels, frequent contact with water and aggressive chemicals from manure or disinfectants.

"For more than 40 years the Euroemme® fan line has risen to the challenges of the agriculture industry and has systematically overcome each new hurdle. Today we see that the housing is cutting fan life short, which is why we offer Munters Protect. All Munters' metal fans from our factory in Italy will from now on be coated with Munters Protect", says Director of Product Management, Giacomo Bergui.

Benefits of Munters new coating

  • The best corrosion resistance performance, up to 10 times better than galvanized steel
  • The best suited protection, known to market, to withstand harsh environments as in livestock buildings and greenhouses
  • An extended warranty of 3 years on the fan housing and shutter blades (excl. swine applications)

Long lasting material means longer product life-cycle and less maintenance on fans, reduced total cost of ownership.

For more information, please contact:

Catherine Brynielsson, Global Market Communications Manager,

e-mail: catherine.brynielsson@munters.se

Munters Europe, PO Box 1150, Isafjordsgatan 1, S-160 40 KISTA Phone: +46 8 626 6300

Munters develops and manufactures energy efficient climate control systems for the growth and development of agriculture and horticulture applications. By providing the perfect climate, our solutions enable farms to operate and produce under optimum conditions. The innovative product range includes ventilation, cooling, heating and cutting-edge control systems. Munters always strives to be the premium partner for our customers. www.munters.com

우리는 전문가 입니다

우리는 우리의 제품을 알고있다. 우리는
귀하의 국가에서 사람을하여
연락처 정보를 안내합니다