chrysantemum1.jpg

Munters improves production for flower grower

6 10, 2014

Greenhouse manufacturer Asthor Agrícola S.A. complete “turnkey” horticultural projects, and cooperate with Munters for climate control of its greenhouses. A recent joint project in Obidos, Portugal showed great results for the customer.

Quinta do Sitio da Cruz, a family-owned business, was faced with the need to increase and improve production in its flower greenhouses, and after having installed a number of units with equipment by another brand, they decided to choose Munters climate control system in the latest greenhouse.

After one year of operation, the differences between the unit fitted with Munters climate control system and the other greenhouses are considerable. The temperature and humidity conditions inside the greenhouses are more homogeneous, while the durability of the pads is greater as they stay cleaner, with no algae or organic deposits.

"The CELdek pad improved the performance with a lower air speed and less electricity consumption", commented Osvaldo Branco from Quinta da Sitio da Cruz.

Adding to the sustainability aspect is the special fan shutter mechanism which prevents air leakage through the fan, enabling an hermetically sealed environment. This way, fans and cooling pads operate only when needed, and electricity consumption is kept down to a minimum.

Many years of experience in the manufacture and application of climate systems has clearly proved to Munters that climate control – based on the "pad and fan" cooling system as well as on our air-heating systems – is the most efficient and trustworthy technology available. And this is true both for boosting production and for cutting costs, not to mention operational reliability.

우리는 전문가 입니다

우리는 우리의 제품을 알고있다. 우리는
귀하의 국가에서 사람을하여
연락처 정보를 안내합니다