Munters AB has divested its FoodTech Equipment offering to Grain & Protein Technologies, owned by American Industrial Partners. As a result, neither Munters AB nor any of the companies within the Munters Group are responsible or liable for any content related to FoodTech Equipment that temporarily remain on the website or for any products or services related to FoodTech Equipment, except to the extent required by applicable law. This includes any inaccuracies, errors, or omissions in the information provided. For more information, please refer to the press release dated 9 February 2025, available at https://www.munters.com/en-us/news-media/press-releases/2025/munters-signs-an-agreement-to-divest-the-foodtech-equipment-offering/.

Lavamatic
ムンタースLavamaticドラムウォッシャーは、鶏舎や豚舎の排気から発生する粉塵やアンモニアの排出を削減します。豚舎では、追加の生物学的ステージによる臭気低減が可能です。この完全な組み立て済みモジュールは、50,000 m3/hと100,000 m3/hの2つのサイズで利用でき、家畜農家の環境規制遵守に役立ちます。
Highlights
- アンモニア排出量を80%以上削減
- 排気中の粉塵を最大90%除去
- 臭気を最大300 GE/m3まで低減
- 低エネルギー消費量と優れた操作安全性
- 簡単なメンテナンスとクリーニング
- 独自の回転式洗浄ドラム
このシリーズの製品
モデル | 製品シート |
---|---|
Lavamatic | 表示 |