Siamo esperti

Si è verificato un errore durante l'invio del messaggio, per cortesia riprova più tardi

Fai una domanda

Munters Protect the barrier against corrosion

lug 4, 2014

Munters moves away from galvanized steel for the metal fan line and now launches Munters Protect. The implementation of the new anti-corrosion material forms another step in Munters quest of safeguarding that our products stand the test of time and last in the environment where they are placed, while ensuring that the environmental footprint is reduced.

Step by step with continuous improvements

The agriculture environment is challenging to metal products and corrosion is caused by many factors such as pH, high humidity levels, frequent contact with water and aggressive chemicals from manure or disinfectants.

"For more than 40 years the Euroemme® fan line has risen to the challenges of the agriculture industry and has systematically overcome each new hurdle. Today we see that the housing is cutting fan life short, which is why we offer Munters Protect. All Munters' metal fans from our factory in Italy will from now on be coated with Munters Protect", says Director of Product Management, Giacomo Bergui.

Benefits of Munters new coating

  • The best corrosion resistance performance, up to 10 times better than galvanized steel
  • The best suited protection, known to market, to withstand harsh environments as in livestock buildings and greenhouses
  • An extended warranty of 3 years on the fan housing and shutter blades (excl. swine applications)

Long lasting material means longer product life-cycle and less maintenance on fans, reduced total cost of ownership.

For more information, please contact:

Catherine Brynielsson, Global Market Communications Manager,

e-mail: catherine.brynielsson@munters.se

Munters Europe, PO Box 1150, Isafjordsgatan 1, S-160 40 KISTA Phone: +46 8 626 6300