Siamo esperti

Si è verificato un errore durante l'invio del messaggio, per cortesia riprova più tardi

Fai una domanda

HartlGroup_OasisOutdoor_spotcolour.jpg

Hartl Group

set 16, 2016

Hartl Group was founded in 1992 by Peter Hartl, and is headquartered in Hofkirchen, Lower Bavaria Germany.Being one of the leading IT service providers in the area, Hartl Group is offering services like consulting and auditing, process optimization, Data Centre hosting in Austria and Lower Bavaria, user helpdesk, training, network and communication.

In March 2016 a brand new Data Centre was inaugurated in Hofkirchen to replace older facilities no longer up to date. The new Data Centre features the most modern solutions within safety, energy efficiency and storage solutions.

The Data Centre is hosting data for smaller and bigger local companies, banks etc. and will be able to contain 64 racks and work with an IT load of up to 600 KW.

Striving for a low PUE

During the planning of the new Data Centre, Peter Hartl got in contact with Munters in his search for an energy efficient cooling solution.

Striving for a PUE as low as possible, Munters’ indirect evaporative cooling system Oasis™ could form the perfect solution.

Compared to a traditional DX based cooling solutions for Data Centres, the Oasis™ solution typically saves up to 75% energy. Mainly due to the elimination of compressors and also thanks to the reduced need of fans involved.
Munters worked out a design with two Oasis™ 200 units that would be able to satisfy the requirement of strictly controlling the temperature within the Data Centre between 23-25°C around the year.

Read the full case study