Munters solutions in Onur pullet farm

dic 11, 2015

The Onur pullet farm is located in Çorum, Turkey and is owned and operated by the Yürüyen and Öz families. The farm produces three million pullets per year.

Even though the outside climate is not ideal for growing chickens, Munters was able to combine a system, using our product portfolio that can provide the ideal indoor climate to the chickens for all seasons of the year.

A combination of exhaust fans, cooling pads, climate controller, wall and light inlets have been installed to assure the perfect climate inside the farm for a stable production, stress free birds, reduced mortality rates and improved feed conversion ratio. The house is fitted with two ventilation systems, one for summer and one for winter but during spring and fall a combination of the two systems is used to make a smooth transition. The heart of the system is the Farm premium controller that controls both systems and decides when to use what components in order to create the ideal indoor climate.

The IW wall inlets assure an optimal growth for the birds by providing even air distribution. Light filters reduce the light intensity inside the house sufficiently utilizing artificial daylight programs to full effect. The exhaust fans assure a smooth air flow and the CELdek pads provide highly efficient cooling.

Watch the video below for a visual experience of the farm and don’t forget to SUBSCRIBE to Munters Youtube Channel, like and share.

List of the products installed by Munters:

1) TU exhaust fans

2) CELdek cooling pads

3) EC50 Exhaust fans

4) Farm premium controller

5) IW wall inlets

6) LFD light filters