Une erreur occursée lors de l'envoi du message, s'il vous plaît essayer à nouveau plus tard
Une erreur occursée lors de l'envoi du message, s'il vous plaît essayer à nouveau plus tard
The Munters RPLP-1 provides lightning protection to Munters Controllers. Refer to the RPLP-1 documentation for detailed wiring instructions. While no lightning protection is perfect, the RPLP-1 significantly enhances the reliability of built-in lightning protection. In addition, Munters recommends using the RiT-50 Isolation Transformer in front of the RPLP-1 to help block lightning and other transients.
The following diagram illustrates how to wire the RPLP Lightening Protector and power equipment (such as fans or heaters) to a controller. The drawing below shows a SMART-C card. However, the principles apply to the Munters AC-2000 and Pig Guard Controllers.
CAUTION To ensure proper operation, verify that power to the controller is via the RPLP ONLY! Power to the contactors (1 or 3 phase) and the variable fan must come directly from the power line.
The following diagram illustrates how to wire the RPLP Lightening Protector, RIT-50 Isolation Transformer and power equipment (such as fans or heaters) to a controller. The drawing below shows a SMART-C card. However, the principles apply to the Munters AC-2000 and Pig Guard Controllers.
CAUTION To ensure proper operation, verify that power to the controller is via the RPLP and RIT-50 ONLY! Power to the contactors (1 or 3 phase) and the variable fan must come directly from the power line.
Identifiant invalide
Oups! Une erreur est survenue. Essayez plus tard.
Mot de passé oublié?
Identifiant invalide
Oups! Une erreur est survenue. Essayez plus tard.
Check your email within a couple of minutes to reset your password, if you can’t see any incoming messages try to check into your spam folder!