Ha ocurrido un error cuando se ha enviado el mensaje, por favor, inténtelo más tarde
Ha ocurrido un error cuando se ha enviado el mensaje, por favor, inténtelo más tarde
The Munters RPLP-1 provides lightning protection to Munters Controllers. Refer to the RPLP-1 documentation for detailed wiring instructions. While no lightning protection is perfect, the RPLP-1 significantly enhances the reliability of built-in lightning protection. In addition, Munters recommends using the RiT-50 Isolation Transformer in front of the RPLP-1 to help block lightning and other transients.
The following diagram illustrates how to wire the RPLP Lightening Protector and power equipment (such as fans or heaters) to a controller. The drawing below shows a SMART-C card. However, the principles apply to the Munters AC-2000 and Pig Guard Controllers.
CAUTION To ensure proper operation, verify that power to the controller is via the RPLP ONLY! Power to the contactors (1 or 3 phase) and the variable fan must come directly from the power line.
The following diagram illustrates how to wire the RPLP Lightening Protector, RIT-50 Isolation Transformer and power equipment (such as fans or heaters) to a controller. The drawing below shows a SMART-C card. However, the principles apply to the Munters AC-2000 and Pig Guard Controllers.
CAUTION To ensure proper operation, verify that power to the controller is via the RPLP and RIT-50 ONLY! Power to the contactors (1 or 3 phase) and the variable fan must come directly from the power line.
Identificación de Usuario Inválida
Ups! Algo salió mal. Por favor intenta nuevamente
¿Olvidaste tu contraseña?
Identificación de Usuario Inválida
Ups! Algo salió mal. Por favor intenta nuevamente
Check your email within a couple of minutes to reset your password, if you can’t see any incoming messages try to check into your spam folder!