Sustainable and accurate climate management in the Learning and Innovation Center Archive
In the construction of the Learning and Innovation Centre (LIC) in the Vrije Universiteit Brussel (VUB) and the Université Libre de Bruxelles (ULB), accurate climate control for the archive rooms was critical.
Munters was selected by Arcadis, the world's leading company delivering intelligence-driven sustainable design, engineering, and consultancy solutions for natural and built assets, as the ideal partner to provide an energy-efficient and reliable solution to preserve valuable documents and materials.
‘Sustainability was paramount in the construction of the LIC, both in terms of material use and energy consumption. Our goal was to minimize energy consumption, which led to several things including improved ventilation, where Munters made a big difference.’ - Thomas Haustraete, Project Manager at VUB
The recipe for the perfect archive climate

Expertise through all phases of the project
"Munters is not only a supplier of essential climate technology, but also actively thinks along with the customer. That makes us strong. The LIC project is a great example of this: determining the right concept was a challenge, but we are proud to have been involved from design to delivery.
We continuously invest in our R&D department to develop environmentally friendly and energy-efficient solutions. From our position as a manufacturer, we are constantly looking for what the market needs and how we can tailor our development and innovation accordingly."
- Wouter Adriaens, Applications Engineer at Munters

Versatile ventilation for archive rooms
Today, an ML1100PLUS system is installed in the archive room of the LIC: a modular climate system that can cool, heat, humidify, and dehumidify the room in a highly energetic way. The Vrije Universiteit Brussel had set strict performance standards with very specific limits for humidity and temperature:
- The LIC archive standards are 18 °C and 45% RH (relative humidity).
- Stable conditions of 1 °C and 3% within a 24-hour period.
- Keep fluctuations to ±2 °C and 5% over a longer term
Thanks to the ML1100PLUS' precise cooling and heating coil, humidifier and dehumidifier, the room always remains within these standards without any problems.
The application of the ML1100PLUS is very diverse. The system is ideal for storage rooms and archives, such as those at the LIC, but has also been proven in museums and galleries, clean rooms and laboratories, for food production, and for packaging, filling and capsule rooms in pharmaceutical and industrial processing lines
‘Together with Wouter Adriaens of Munters, we at Arcadis determined how the air group should be constructed and perform. We also looked together at the overpressure and airtightness in the archive. The cooperation went very smoothly, both in design and execution. This was clearly a successful collaboration!’ - Vera Desoppere, Senior project engineer at Arcadis
What makes this ventilation solution so special?
Want to improve your indoor climate?
Whether you're in pharmaceuticals, food production, battery manufacturing, or preservation, Munters delivers tailored solutions that ensure optimal performance across industries. Simply click the "Talk to an expert" button below, fill out our contact form and one of our air treatment specialists will be in touch to help you find the right solution.