Dovolte, abychom vám pomohli

Při odesílání zprávy došlo k chybě, opakujte akci později.

Položit otázku

Phil_Nissan_Case.jpg

Plug fan upgrade pays back in only 21 months

Upgrade of belt driven process fans and motors cut energy consumption by 30%

“With the update we are increasing the capacity of the units for the same amount of energy used. It offers us more redundancy and gained resilience”

- Facility Engineer Phil Laing at Nissan expresses great satisfaction with the project.

Nissan's Sunderland plant in the UK is the biggest automotive manufacturing facility in the country, producing more than 500,000 vehicles a year and employing over 6,500 workers.

Nissan has been heavily investing to support facility expansion, new model line-ups and job creation. NMUK produces the Nissan Qashqai, Note and Juke and the 100% electric Nissan LEAF as well as lithium-ion batteries at its battery plant. The Nissan LEAF made history as the world’s first affordable, mass-market, 100% electric vehicle. Powered using lithium-ion battery technology, these innovative vehicles make no noise and emit zero emissions. To produce the batteries needed to power these electric vehicle, Nissan’s plant in Sunderland built a 25,000 m² clean/dry room that requires very precise and constant climate conditions.

Munters strictly controls climate

Munters ensures this area is held at
-55°C dewpoint with 100% fresh air, by using three MDU2500 gas reactivated desiccant dehumidification units fitted with pre and post treatment. Designed to meet the specific requirements stipulated by Nissan, the systems were commissioned in 2011 and maintained by Munters Service.

Focus on energy savings

To ensure Nissan car plant remains productive and efficient, the Nissan Facilities teams are always looking for projects that can save energy, reduce CO2 emission and costs. These projects will need to provide return on investments (ROI’s) in less than 2 years.

Since Munters Service is dedicated to helping customers optimise the value of their air treatment equipment, different options for energy optimisation on Nissan's MDU dehumidification systems were investigated.

Fan/motor upgrade
Due to advances in fan and motor technology, it became apparent to Munters that it would be beneficial to NMUK to update the original belt driven process fans and motors in the MDU’s with newer and more energy efficient direct drive plug fans fitted with IE3 motors. After surveying and installing data loggers Munters were able to provide estimated energy savings and an average ROI of twenty one months across the project, which was well within the client’s stipulated ROI of two years.

The project involved upgrading the three Munters’ MDU2500's systems and also three McQuay air handing units with direct drive plug fans. The existing Munters systems were originally fitted with belt driven fans driven by 15kW motors, and because of the efficiencies gained by direct drive plug fans it was possible to replace one 15kW motor with two 5,5kW plug fans for each system. The increased capacity and redundancy are important advantages in a manufacturing plant, constantly striving to optimise production processes. In total Munters will save the client 47% of the fans running costs on the three dehumidification systems. In addition there will be less maintenance to be done, as there are no belts and pulleys to change and service.

Upgrades also on AHU systems
In general the conversion from belt driven fans to direct drive plug fans reduces the energy consumption by 30% and Munters Service offers these upgrades not only on older Munters’ MDS and MDU dehumidification systems, but also on non-Munters conventional air handling units. Contact your local Munters Service Team and we will assist you in calculations on estimated energy savings in your specific case.

Read more about our Service Products
Munters Global Services

CONTACT US
Fill in the Contact box on your right hand side to get in touch with your local Munters Service Team and we will assist you in calculations on estimated energy savings in your specific case.
Or find your local office here:
Munters Global Offices

Stručná fakta

  • Upgrade reduces fan/motor energy consumption by 30%
  • Short return on investment - only 21 months
  • Reduced maintenance costs
  • Better control and more redundancy