AHR Exhibition 2010 Orlando, FL

The drive for greater energy efficiency, greener products and sustainable technologies has accelerated the pace at which new products and innovations are coming to market.  In this challenging economy, HVAC & R professionals must also be more innovative in their businesses or be left behind. 

That’s why AHR Expo is the one event you don’t want to miss.  Munters Humicool will be presenting in the show floor 2 of their climate control solutions for the industry.

EPCC Evaporative PreCooler Condenser, a balance between cooling function, cost and energy. Air-cooled refrigeration units are the typical form of heat rejection systems used for air conditioning, ventilation and refrigeration today. Adequate cooling must be balanced between capital investment cost and physical installation space. In addition to operating costs, maintenance and rising energy costs as well as environmental impact (CO2 emissions) are critical factors.

Also in the show floor of the exhibition you will find the Munters DropSTOP droplet separator is highly efficient, it has been specially developed and optimised to remove droplet carry-over from cooling coils. DropSTOP droplet separator consists of GLASdek 3 media that is integrated into a stainless-steel cassette. GLASdek 3 media is a glass-fibre-based material that is non-flammable, elastic and easy to handle. The material is highly absorbent, with a capacity corresponding to 100 litres of water per cubic metre of media.

If you would like more information about this products please contact our sales representatives in booth: 2900


 

Related information

Kontakt
Lars Engström
CEO                             
Tel: 08 626 63 03
Mob: 070 228 85 19
>>Epost

P-A Håkansson
VP Corp. Communications
Tel: 08 626 63 82
Mob:  0702 38 68 82
>>Epost

 
  • Munters AB | Isafjordsg 1, Kista Entré | P.O. Box 1188 | S-164 26 Kista| Sweden | Reg no 55 60 41 - 06 06 | © Munters 2011