HER - Next generation of mobile heaters

HER - Next generation of  Mobile indirect fired heaters from Munters Sial.  Versatility, flexibility, efficient logistics in a robust and powerful designed heater was the base for this new release of Munters Sial, which is giving over 90% of efficiency. The new heater is directed for the construction market has also other applications for indoor temporary heating.

Munters Sial, in the continuous commitment with improvement of their product lines, has a new product to be released to the market this autumn 2009.

New heater soon to be released
Sial, a company that has been on the market since 1973 and that has been leader in the European market, was acquired in 2006 by Munters, a global company leader in climate control solutions that at the same time are environmentally friendly. Munters Sial research and development department has lately been working on HER, a new mobile indirect fired heater, which will be presented to the market on the following SAIE International Building Exhibition, which will take place in Bologna Italy from October 28th through 31st 2009.

Robust, Powerful and efficient heating
Versatility, flexibility, efficient logistics in a robust and powerful design, was the base for this new release of Munters Sial heaters. The new heater which is mainly designed for the construction market is also suitable for other applications for indoor temporary heating, such as temporary events, marquee heating. The new release will be presented in 100kW, 130 kW, 160 kW and a larger unit of 220kW to be released next spring. Being HER an indirect heater allows it to run on a close space with people permanently present. The usage of this heater for concrete drying is another application to be approach with this new versatile indirect heater. Due to its heavy duty design is ideal for construction sites.

Special features
The new HER will bring to the market a robust, heavy duty heater, available in different fuel options (Oil, Diesel, LPG, Natural Gas), with the perfect size to go though doors in the building. It is ideal for indoor temporary heating, but thanks to its power centrifugal fan it is suitable to be used outdoors and the air ducted in as well. Wheels, retractile handle and a special frame make this heater easy to handle and move around the building.

Related information

Contacts
Lars Engström
CEO                             
Tel: +46 8 626 63 03
Mob: +46 70 228 85 19
>>E-mail


P-A Håkansson
VP Corp. Communications
Tel: +46 8 626 63 82
Mob: +46 702 38 68 82
>>E-mail

  

 


   

 
  • Munters AB | Isafjordsg 1, Kista Entré | P.O. Box 1188 | S-164 26 Kista| Sweden | Reg no 55 60 41 - 06 06 | © Munters 2011