Global

Mist elimination

Mist elimination is a technique that removes undesirable drops of moisture from gas or air.

Munters’ mist eliminators are based on a unique technology in which the gas passes through small ducts that capture and remove the drops. The most important application area is cleaning emissions from coal-fired power plants.

The flue gas is sprayed with water that contains chemicals that capture the contaminants in the smoke. Thereafter, the water containing the contaminants is removed with Munters’ mist eliminators.

 
  • Munters AB | Isafjordsg 1, Kista Entré | P.O. Box 1188 | S-164 26 Kista| Sweden | Reg no 55 60 41 - 06 06 | © Munters 2011