Global

Core technologies

Munters' business is based on fundamental relationships between water, air, and energy. Changes in any of these elements will immediately have an affect. Such are the laws of nature.

Different climates create different prerequisites
The relationship between the components of dry air is constant in all parts of the world. The amount of water in outdoor air, varies significantly however. The higher the temperature, the more water vapor the air can contain. This means that the relative humidity indoors is lower than the outside air when premises are heated and higher when they are cooled.

Because humidity can increase when a room is cooled, air conditioning, contrary to what many people believe, create humidity problems in many situations. In warm climates, air conditioning and dehumidification are therefore required, while cold climates need heating and humidification.

In common for every climate
What every climate has in common is the need to regulate both temperature and air humidity. For companies with business operations in different climates, it is important to ensure that products maintain the same quality, regardless of where they are manufactured.

Based on these everyday requirements Munters continually refines its product and system offering.

Munters has a number of core technologies:

  • Dehumidification
  • Air cooling and heating
  • Humidification
  • Heat-exchange technology
  • Mist elimination
  • Contaminant elimination

 
  • Munters AB | Isafjordsg 1, Kista Entré | P.O. Box 1188 | S-164 26 Kista| Sweden | Reg no 55 60 41 - 06 06 | © Munters 2011