When Corporate IT at the University in Copenhagen, Denmark, was about to bring all their servers into two large server rooms, the Consulting Engineers at EKJ A/S were looking for a new and more energy saving solution. Since the servers contain important research data, the ideal server room climate is of vital importance and reliability and fire safety are high priorities.
By installing 4 Munters air conditioning units for cooling the server rooms, the University of Copenhagen has been a frontrunner in changing common practice in cooling server rooms to achieve substantial energy savings.
EKJ Consulting Engineers AS compared 4 different methods of cooling and the investment in Munters system turned out to be at least 25% cheaper compared to traditional solutions, as well as the most energy efficient solution. Energy costs are estimated to amount to only 50% of the running costs of a traditional cooling/downflow solution.
With Munters climate control in the server rooms are secured.
- without any refrigerants
- without compressors
- with no need of additional chillers