MCS

 Morten Andreasen, Division President MCS

Munters’ MCS division offers services in damage restoration after water and fire damage, primarily for insurance companies – in addition to humidity and temperature control for the construction industry and others.

Operations are conducted on a global scale, with a strong local presence in 260 service depots. MCS has rapid response times and efficient and environment-friendly technology. MCS creates value by minimizing costs in terms of the extent of damage and its management, as well as by managing the damage professionally and securely with the insurance policyholder. In the area of temporary humidity and temperature control, value is created primarily by means of high-quality services and by cutting the time required for the customer’s project .

Damage restoration

Munters offers cost-effective and environment-friendly restoration of damage of highly varying types. High availability, short input periods, modern technology and efficient processes are valueadding competitive advantages that Munters can offer customers through its size and accumulated experience in the area. Damage restoration is conducted in all conceivable environments, from the restoration of individual buildings to large-scale commercial damage and restoration following major individual events. The division also offers preventive services such as the Code BlueTM program.

Temporary humidity control

Munters also offers services that involve temporary humidity control at sites in which air humidity is a problem. The technology is applied to eliminate corrosion during surface treatment and to limit or prevent disruptions in production processes in connection with construction and maintenance work. Productivity during construction is increased thanks to faster drying and the ability to continue working regardless of weather conditions. The solution is cost effective in that installation is temporary and energy-effective products are used.

Search