Welcome to Munters news room. To keep updated with what is happening, you can subscribe to our news.
Aug
13, 2008
- Second quarter
Order intake amounted to SEK 1,686 M (1,688) – up 4% adjusted1
Net sales advanced 2% to SEK 1,548 M (1,524) – up 5%,
Costs for the MEP2 program (Munters Efficiency Program phase 2) totaled...
Aug
11, 2008
- Jonas Samuelson, currently Chief Financial Officer (CFO) of Munters AB, has accepted an offer to take up the position as CFO for Electrolux. The transition will take place before end of 2008. The recruitment of his...
Jul
29, 2008
- Munters AB will be holding a presentation and conference call following the results of the second quarter 2008. Mr. Lars Engström, CEO and Mr. Jonas Samuelson, CFO will deliver an update on the progress during January -...
Jul
10, 2008
- Munters has entered into an agreement to acquire Belgium-based Toussaint Nyssenne, manufacturer of high quality air conditioning systems, complementing Munters energy-efficient air treatment product range. The company...
Jul
9, 2008
- Munters acquires Västgöta Torkteknik AB and further strengthens its position as leading service provider within water damage restoration in Sweden. Information on the transaction is not considered stock price...
May
27, 2008
- Munters has decided to change the release dates for the coming two interim reports as well as established the date for the year-end report.
Munters has set the following dates:...
Apr
22, 2008
- Full report (pdf)
Order intake rose to SEK 1,586 M (1,527), up 4% - up 2%, 2%, adjusted1
Net sales advanced to SEK 1,545 M (1,404), up 10% - up 7%, adjusted1
Costs for the MEP2 program (Munters Efficiency Program...