Munters MCS - Leak Detection Services

Packaging industry has serious problems when the winter comes due to the low relative air humidity in the packing hall. The dry air affects the shape of the
cardboard sheets which are used to make boxes. The packing machine is extremely sensitive to changes in shape, the result being excessively high cardboard wastage.

The benefits of installing a Humidification system of Munters are:

  • A constant, regulated air humidity in the packing hall – cardboard sheets retain the correct structure.
  • No static electricity that can cause machine stoppages.
  • No chalk dust spread in the air, which can otherwise settle on walls and machinery.
  • The air humidifier has a low power requirement (50-250 W).
  • Excellent adjustability.
  • Easy maintenance and low running costs.

A Munters air humidifier with step regulation installed in the packing hall’s ventilation system can change a previous level of 15-20% RH, to a relative air humidity of  50%, which eliminates problems of shape changes in the cardboard sheets and removes the static electricity build-up. Cardboard wastage is also reduced.

See how our humidifier helped V & S Group with their biggest brand ABSOLUT

 

  • Munters AB | Isafjordsg 1, Kista Entré | P.O. Box 1188 | S-164 26 Kista| Sweden | Reg no 55 60 41 - 06 06 | © Munters 2011